The BCS e-bike charging station
Mobility is becoming more and more climate-conscious
All our efforts are to reduce CO2 emissions, the market for LEV (Light Electric Vehicles) is experiencing a real boom. Almost a million e-bikes were sold in Germany in 2018.
And the trend continues:
A market analysis by BOSCH predicts that in 2027 every second bicycle will have an electric drive. There are also segways, e-scooters, e-scooters and other micromobiles.
For these it is important to create the necessary charging infrastructure. The charging plugs from the e-bike manufacturers are not standardized. Currently E-bikers have to carry their chargers accordingly to stay mobile. With the new BCS, there is no need to carry the charger with you!
E-bikes in Germany
Over 7 million e-bikes on the streets
In 2020, approx.
2 million e-bikes sold
Currently around 7400 charging stations available
Modular e-bike charging station
Offer your customers or employees an additional service. The innovative and extremely robust GEOS housing is basis for the charging station. In the standard configuration, the BCS e-bike charging station is equipped with original charging systems from Bosch and Shimano as well as SCHUKO sockets. The use of original components ensures high reliability. This makes it possible to charge an e-bike even when the charger is not at hand. The cable management ensures that the variety of connections is easy and safe to use. Additional convenience is provided by an LED status display, the mounted cable holder and a large operating temperature range for year-round use of the charging station in a protected outdoor area.
The ready-to-connect e-bike charging station BCS is the perfect solution for
- Utilities and municipalities
- Chain stores (hotels, discounters, drugstores etc.)
- Cafes, bars and restaurants
- Small & medium Enterprises and industry
- Tourism branch
The variants of the e-bike charging station BCS in comparison
BCS Pure
- Bosch & Shimano
- 4
- -25°C bis +40°C
- 16 A (On the building side)
- Fixed mounted, 2,5 m
- 2x Cable holder, fixed on the outside
- IP 54 / IK 08
- 2x Schuko®-sockets 230V
- immediately
BCS Smart
- Bosch & Shimano
- 4
- -25°C bis +40°C
- 16 A (On the building side)
- Fixed mounted, 2,5 m
- 2x Cable holder, fixed on the outside
- IP 54 / IK 08
- 2x Schuko®-sockets 230V
- over the year
BCS-Management portal
As an operator of an e-bike charging station, the portal offers you several advantages
The web-based portal for the e-bike charging station BCS Smart from Spelsberg offers you as the operator of the charging stations comprehensive functions.
The management portal for the BCS Smart version is available free of charge for 24 months.
The web-based management portal provides an overview of all installed BCS Smart charging stations. How many loads have been carried out and when? How many users use a charging point? Do you need maintenance? Activate and deactivate the e-bike charging station. The BCS Portal gives you a quick and easy overview of a number of services and other questions. This gives you an insight into the status of the charging stations and user behavior.
Spelsberg TG BCS 3
Spelsberg has been serving the e-bike market segment with its own products for years:
The TG BCS 3 is the previous version of our e-bike charging station BCS Pure and BCS Smart.
As a ready-to-connect solution, today's entry-level version offers a housing of the usual high Spelsberg quality that has already been fitted with three Schuko sockets. The solution is made of durable polycarbonate and extremely robust. The special cover screws prevent unauthorized opening of the housing. A ventilation plug ensures that there is no condensation inside.
The associated weather protection roof made of stainless steel, which is available as an accessory and can be installed sabotage-proof this offers perfect protection for outdoor installation. If you cannot mount the station on a wall, you will find the right alternative with an earth spike, which can also be ordered as an accessory. The sturdy stainless steel spit can be concreted in, whereby the cables are routed invisibly through the interior. Threads for fastening the weather protection roof already exist here and the necessary screws are included.
The special highlight of the station is its customizability: Spelsberg also offers printing according to customer requirements, so that the appearance can be individually adapted to the operator or location. From the company logo to colorful pictures, everything is possible in the in-house printing service center at the headquarters in Schalksmühle. The translucent material of the lid opens up even more possibilities for optical effects. Here, too, customer requests, such as lighting the station, can be implemented individually.
The TG BCS 3 is also available in an illuminated version.