• Products
  • Pages
  • News
  • Distributors

Technical information for concrete installation

Pictograms

Protection class (IP-Code)
as per DIN EN 60529 (VDE 0470-1)

Products for the use in
concrete construction
as per DIN VDE 0606-1

Suitable for the use in concrete.
Resistant to short-term temperatures
up to +90°C during the curing process.

Suitable for LED lamps

Suitable for the installation of lamps
in which cold-light mirror lamps
(cool-beam reflectors) can be installed.
They reduce the thermal load in the
light beam.

Halogen-free enclosure,
without halogens such as fluorine,
chlorine and bromine

The VDE mark stands for approved
safety of the product referring electrical,
mechanical, thermal and other hazards.

Overview of the ambient conditions and mechanical properties of the IBT products

 Enclosure without fittingsEnclosure with fittings
Ambient temperatureMax. relative humidity
 Min.Max.Average over 24 hMin.Max.Average over 24 hat 40°Cat 25°C (short-term)Protection rating according to DIN EN 60529 / VDE 0470-11)Shock-proof as per DIN EN 50102 / DE 0470 Teil 100
IBT / IBTronic
concrete installation system
-25°C40°C35°C-25°C35°C25°C50%k.A.IP30k.A.

Additional note: The specified temperatures may be limited by the installed devices.

1) When used with suitable connectors or cable screw couplings

Overview on the properties of the materials used in the IBT products

MaterialUsed in the products

Weak acids

Strong acids

Weak alkalis

Strong alkalis

Alcohol

Petrol

Benzene

Mineral oil

Diesel

Ammonia, gaseous
(DLG-Focus Test)

Vegetable fats

Animal fats

Halogen-free

Heavy metal-,
PVC- and silicon-free

Combustion behaviour 
DIN EN 60695
(VDE 0471) / UL94

Polystyrene,
impact proof
UP 015-Verteilerset
Verschlussdeckel K
oøoooxxøxoøønoyes960°C / V-2
PolypropyleneIBT sockets + boxes
IBTronic, IBTronic-TT,
IBTronic XL, IBTronic XL
Drillbox, IBTronic XL
Drillbox 150, Precon,
IBTLED
oøoøoøøøooooyesyes650°C / HB
Polycarbonateconduit adapteroxxxoøxoøooøyesyes960°C / V-2

o = resistant  /  ø = conditionally resistant  /  x = not resistant

1. Large-panel construction

means the industrial production of wall and ceiling elements in the concrete plant and is carried out by pouring the concrete in formworks when laying down (horizontal) or standing upright (vertical) (battery moulds, vibration and tilting tables, etc.). The precast concrete elements are transported to the construction site and assembled there. The construction of the partial prefabricated ceilings (filigree floor) saves the slab formwork on site. The installation sockets U86 and U12, for instance, are inserted in the filigree floors. They protrude beyond the ceiling slab and are provided with installation conduits on-site at the construction site. After that, concrete is grouted in until the full height is reached.

2. In-place or heaped concrete construction method are individual installations on site

In doing so, a difference is made between laying (e.g. slab formwork) with only one formwork side and standing formwork with two formwork sides (work formwork with opposing formwork).

Working formwork

Ideal, because the installation of sockets and boxes on the first, already standing formwork (working formwork) can be done easily and fast. After the system has been connected to the conduits and the steel reinforcement has been inserted, the second form (opposing formwork) is put to wall distance. After concrete has been grouted and has cured, the working formwork is removed and with this, the front side of the sockets and boxes is separated. Now the insertion devices (switches and sockets) can be mounted.

Backing formwork

If sockets and boxes are installed opposite the already existing formwork, this is called opposing formwork. For this purpose, first the blank bases are mounted on the working formwork; then, the sockets and boxes are put to wall distance using the support beams. In doing so, the support spar length is always “wall thickness minus 1 cm”, independent which sockets or boxes are used! Only the wall thickness determines the length of the support beams! The necessary stability of the system is achieved by the pressure that is applied by the formwork “moving against it”.

Caution: The residence time of the formwork necessary for curing the concrete must be met!

Add product to Watchlists

Existing Watchlists

New Watchlist

organize Watchlist