• Products
  • Pages
  • News
  • Distributors

Solar power charging with control by an external energy manager

"Charging with control by an external energy manager" involves the use of an external management system (EMS), The EMS controls all energy flows in the system, including PV systems, energy storage and loads. Thanks to intelligent control of the energy flows, in the ideal situation only self-generated energy is used as a supply. This significantly increases consumption from own sources and independence from mains power. Please refer to our compatibility list to find out which energy management systems the Spelsberg Wallbox is compatible with.

List of compatible EMS

All parameters are configured via a web-based platform of the EMS. All energy flows are centrally displayed via the energy manager. This allows precise operating times according to the availability of the PV current.

The configuration in the wall box is restricted to the connection with the respective EMS and the associated communication interface. To do this, open the Spelsberg Wallbox app and go to System and then to Settings. Next click System integration and then External control. At this point, you can choose between integration via SMA SEMP, EEBus or Modbus TCP and continue with the configuration as described below. In principle, all devices must be in the same network for integration. Information on network integration can be found here Network integration.

Connection to the Sunny Home Manager 2.0 via SMA SEMP

To configure the Spelsberg Wallbox Smart Pro with the Sunny Home Manager 2.0 via SMA SEMP, follow the settings in the Spelsberg Wallbox app. Detailed information on the various charging modes and the functions of the Spelsberg Wallbox Smart Pro in conjunction with the Sunny Home Manager 2.0 can be found here. The following parameters must be set:

Parameter overview

App Parameter

Settings

SMA SEMP interface

Activate

Automatic phase disconnection

Activate

Dead time: Time taken for pausing the charging process, which should be taken into account when switching between 1-phase and 3-phase charging. A minimum of 60 seconds should be set.

SMA charging mode

Selection:

  • Manual configuration

  • Immediate charging

  • Surplus charging

SMA minimum energy demand [kWh]

Input [0-1,000 kWh]  _ _ _ _ _
(Required for manual configuration charging mode)

SMA maximum energy demand [kWh]

Input [0-1,000 kWh]  _ _ _ _ _
(Required for manual configuration charging mode)

SMA planned departure time

Enter the desired time in the format HH:MM, by when the configured minimum energy demand is to be charged.
(Required for manual configuration charging mode)

Current limitation in the event of failure of the SEMP gateway [A]

Set the maximum charging current (6 - 16 A), in 1 A steps in the event of loss of connection to the Sunny Home Manager 2.0

Once parametrisation is complete, click Apply and transfer the settings to the Spelsberg Wallbox via NFC or network communication.

Connection to an energy management system via EEBus

To configure the Spelsberg Wallbox Smart Pro via EEBus, follow the settings in the Spelsberg Wallbox app. The following parameters must be set.

Parameter overview

App Parameter

Settings

EEBUS interface

Activate

Link EEBUS

When the EEBUS capable EMS is displayed, click "Link" and transfer the data to the Spelsberg Wallbox via NFC

EEBUS charging mode

Selection:

  • Mains charging

  • PV charging (mains and PV power)

  • PV surplus charging

Cost-optimised charging

Activate
(activates the EEBUS Use Case “Self-Consumption Optimisation”)

Charging current in the event of a connection failure [A]

Sets the maximum charging current (6 - 16 A), in 1 A steps in the event of loss of connection to the EMS

Once parametrisation is complete, click Apply and transfer the settings to the Spelsberg Wallbox via NFC or network communication.

 

Connection of an energy management system via Modbus TCP

To configure the Spelsberg Wallbox Smart Pro via Modbus TCP, follow the settings in the Spelsberg Wallbox app. The following parameters must be set.

Parameter overview

App Parameter

Settings

Modbus TCP server

Activate

Modbus register set

Selection:
Phoenix
TQ-DM100
Open Modbus Charge Control Interface (OMCCI)

Allow Start/Stop of charging processes

Activate

Modbus TCP server device address

Input [0-255 kWh]  _ _ _ _ _

Modbus TCP server port

Input [0-65535 kWh]  _ _ _ _ _

Note: Information on the Modbus registers is available on request from our technical service.

Once parametrisation is complete, click Apply and transfer the settings to the Spelsberg Wallbox via NFC or network communication.

 

Add product to Watchlists

Existing Watchlists

New Watchlist

organize Watchlist