Network integration: Spelsberg
  • Products
  • Pages
  • News
  • Distributors

Network integration

To be able to use all functions of the Smart Pro easily and conveniently, a connection to the local area network is strongly recommended. This is possible via Ethernet or WLAN. Make sure that the range of your WLAN extends as far as the location of the wall box. If the range is not sufficient then, for example, a repeater can be used to strengthen the signal. To ensure a stable network connection, use of a LAN cable for the link is recommended.

WLAN

As a user you can configure the connection to the WLAN, by adding the wall box to your Spelsberg Wallbox app. To do so, follow the instructions in the app. Otherwise, open the app and go to "System" - "Settings" to do this. Open "More settings" and show "Expert settings", then select "Network".

Depending on whether a static or automatic network integration is to take place, the following parameters must be set. Parameters for which no setting instructions are given can be ignored in this use case.

Network parameter overview

App Parameter

Settings

 

Auto Discovery

Static configuration

Activate WLAN

Activate

Activate

SSID

Input

 

WLAN password

Input

 

WLAN IP configuration

 

 

WLAN IP address

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

WLAN network mask

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

WLAN gateway

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

WLAN DNS server

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

Ethernet configuration

 

 

Static Ethernet IP address

 

 

Ethernet network mask

 

 

Ethernet gateway

 

 

Ethernet DNS server

 

 

WiFi Hotspot

 

 

WiFi Hotspot password

 

 

WLAN integration - Static configuration

If you wish to perform a static configuration of the WLAN, you must display the expert settings. Open the app and go to System - Settings. Open "Advanced settings" and display "Expert settings". Now select "Network".

The following parameters must be set:

1. "Activate WLAN" parameter

  • This parameter must be "activated"

2. "WLAN IP address" parameter

  • Enter IP address.

3. "WLAN network mask" parameter

  • Enter the network mask.

4. "WLAN gateway" parameter

  • Enter the IP address of the gateway.

5. "WLAN DNS Server" parameter

  • Enter the DNS server. 

Ethernet Integration - Auto

For automatic connection of the wall box via Ethernet a physical connection must first be created between the wall box and the network router using a LAN cable. Chapter 9.9 of the manual contains information on this. As a user you can configure the connection to the WLAN, by adding the wall box in your Spelsberg Wallbox app. Otherwise, open the app and go to "System" - "Settings" to do this. Open "More settings" and show "Expert settings", then select "Network".

Depending on whether a static or automatic network integration is to take place, the following parameters must be set. Parameters for which no setting instructions are given can be ignored in this use case.

Network parameter overview

App Parameter

Settings

 

Auto Discovery

Static configuration

Activate WLAN

Deactivate

Deactivate

SSID

 

 

WLAN password

 

 

WLAN IP configuration

 

 

WLAN IP address

 

 

WLAN network mask

 

 

WLAN gateway

 

 

WLAN DNS server

 

 

Ethernet configuration

Select: Automatic (DHCP) / Static / DHCP server

Select: Automatic (DHCP) / Static / DHCP server

Static Ethernet IP address

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

Ethernet network mask

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

Ethernet gateway

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

Ethernet DNS server

 

Input _ _ _ . _ _ _ . _ _ _ . _ _ _

WiFi Hotspot

 

 

WiFi Hotspot password

 

 

Ethernet integration - Static configuration

For connection of the wallbox via Ethernet a physical connection must first be established between the wallbox and the network router by means of a LAN cable. Chapter 9.9 of the manual contains information on this. For static network configuration via Ethernet, open the app and go to System - Settings. Open "Advanced settings" and display "Expert settings". Now select "Network".

The following parameters must be set:

1. "Ethernet configuration" parameter

  • Select the "static" setting

2. "Static Ethernet IP address" parameter

  • Enter the IP Address.

3. "Ethernet network mask" parameter

  • Enter the network mask.

4. "Ethernet gateway" parameter

  • Enter the IP address of the gateway.

5. "Ethernet DNS server" parameter

  • Enter the DNS server. 
Add product to Watchlists

Existing Watchlists

New Watchlist

organize Watchlist